Other Parts Discussed in Thread: ADS8688, ADS8684, ADS8332
我现在用ADS8688进行ADC转换,通道1输入真正的差分信号0-10V(直流),但是转换后结果变化很乱,只要把AN_1GND接地,数据就很稳定了,而且数据大小正确,请问:ADS8688能输入真差分信号吗?如果可以,我应该怎么接线?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不支持真差分输入,这款相当于单端输入,可以看到negative input命名的均为AIN_nGND。
并且对于模拟输入端的描述中也有提到:The ADS8684 and ADS8688 have either four or eight analog input channels, respectively, such that the positive
inputs AIN_nP (n = 0 to 3 or 7) are the single-ended analog inputs and the negative inputs AIN_nGND are tied to GND.
请问: 功能,接口,性能类似于ADS8688,但是支持真差分的芯片有哪些呢?谢谢
你好,
可以提供一下具体的设计指标吗?比如几路输入,电压范围,需不需要隔离等等,便于选型。
那您看下ADS8332。http://www.ti.com/lit/ds/symlink/ads8332.pdf
你好,我的要求:一路差分模拟量输入,电平0~l0V,直流电压,16位转换,转换速率300k以上,精度越高越好,外围电路简单,spi接口
你好,
可以告知一下对于直流信号需要300k采样率的原因吗?如果是一路信号的话,将差分连接到单端ADC的输入也是可以实现的。
你好,两个问题: 1 上位机发出采样命令后,需要在0.5ms内完成对1路直流信号的采样,所以我随便写了个300K的速率,呵呵 2. 现在应用情况是1路直流电压模拟信号,距离ADS8688有15米左右,这样是否一定的需要差分输入的AD转换芯片?因为距离远,ADS8688这样的单端ADC是否能满足要求?谢谢
你好,
可以提供一下以下几点便于分析问题吗?
1.系统对于电压的采样精度要求是多少?
2.最终的设计需要几个通道的电压采样?如果用8个通道的ADC对一个通道的电压进行会有点资源上的浪费。
3.如果需要多通道采样,要求的每个通道的采样速率是多少?
对于是否可以在长距离的条件下测量电压值,可以利用EVM板进行一个前期的测试,便于得出结论。