Other Parts Discussed in Thread: LSF0108, TLV1117
LSF0108的1.8V使用的是TLV70218,3.3V使用的是1117-3.3
原理如下图所示
测试1.8V这端始终是2.5V。断开A端的这个1.8V,单独测试TLV70218的1.8V没有问题,连接这颗芯片就拉到2.5V
尝试过1.8V输出后加一个磁珠再到LSF0108,还是不行
也尝试将A1-A8全部切掉,不加任何信号,还是不行。
芯片换过,TLV70218换过,都不行
使用了1117-1.8V的电源飞线后,才正常。但是封装不一样啊,用不了。
那么这颗芯片还挑剔1.8V的电源吗,这个我不明白为什么,
还是想使用TLV70218,调试思路?
或者封装可以完全兼容的电源IC,哪科芯片能不出现70218的这个问题?