Other Parts Discussed in Thread: ADS5402
使用ADS5402的同步功能时,有以下疑惑:
1、ADS5402的SYNCOUTP/N信号是在上电配置相关寄存器及0x01的D2(手册上未写)后,就一直连续有输出吗?
2、同步过程如下:SYNCINP/N由一个时钟产生(可以是其中一个ADS的,也可以是其它的时钟?),同时给到每个ADS5402,每个ADS5402要单独检测到SYNCINCP/N信号36个CLKIN周期后数据才开始有效(通过SYNCOUTP/N指示),那么具体操作中每个ADS5402都要用自己的时钟(注意:多个ADS的时钟之间是异步的时钟)检测输出的SYCINP/N,再等36个周期后再检测各自的SYNCOUTP/N信号???这样由于多个ADS的时钟是异步的,采样SYNCINP/N会有问题?
3、请问ADS5402的同步有成功应用吗??具体怎么操作?谢谢!