你好,两个问题: 1 上位机发出采样命令后,需要在0.5ms内完成对1路直流信号的采样,所以我随便写了个300K的速率,呵呵 2. 现在应用情况是1路直流电压模拟信号,距离ADS8688有15米左右,这样是否一定的需要差分输入的AD转换芯片?因为距离远,ADS8688这样的单端ADC是否能满足要求?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
可以提供一下以下几点便于分析问题吗?
1.系统对于电压的采样精度要求是多少?
2.最终的设计需要几个通道的电压采样?如果用8个通道的ADC对一个通道的电压进行会有点资源上的浪费。
3.如果需要多通道采样,要求的每个通道的采样速率是多少?
对于是否可以在长距离的条件下测量电压值,可以利用EVM板进行一个前期的测试,便于得出结论。