Other Parts Discussed in Thread: ADS6445
例如ADC芯片的采样率为100MSPS,位宽16位,那么吞吐量是多少?
用差分LVDS和FPGA相连,FPGA的时钟速率多少能够满足要求/?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS6445
例如ADC芯片的采样率为100MSPS,位宽16位,那么吞吐量是多少?
用差分LVDS和FPGA相连,FPGA的时钟速率多少能够满足要求/?
对于该芯片:
1。采样率是通过输入的时钟控制的。由寄存器控制模式,不同模式支持的最大采样率不同,见table 24, table 12;
2。最高采样率125MHz,则在引脚输入时钟 CLKP/CLKM 125MHz就可以,但必须是2-wire模式;
3。125Msps,14bit 需要用2-wire模式来支持,此时的bit clock = 125M * 14 / 2 = 875MHz,见table 24; 若FPGA数据位宽16bit,您可以选择以16位一帧,也就是一个字长的形式来传输,其高两位会是0,时此的bit clock 是125M * 16 / 2 =1000MHz;
另,寄存器配置可通过SPI接口实现,该芯片SPI支持的最大速率是20M。
如该回复对您的疑问有帮助,还请确认下,谢谢。