Other Parts Discussed in Thread: ADS1294
各位好,
我将ADS1294用于数据采集,使用内部时钟和内部振荡器。在PCB设计中,我将CLKSEL直接固定为高电平,并且RESET和PWDN短接在一起,由MCU控制复位时序。
上电后先进行复位,然后读取ADS1294的ID,然后设置ADS1294的采样率为1Ksps。
在这个过程中偶尔出现实际采样率与设定采样率之间存在3%的固定偏差。比如:设定1Ksps,实际采样率(从data ready 引脚测得)约为970Hz。设定250Hz,实际采样率242.5Hz。
而且还发现,读ID的时候,理论上应该读到0x90,但有时候返回的是0x80,当返回0x80的时候后面测得的采样率就一定会出现3%的偏差。这两个现象总是成对出现。
另外补充一点,返回值0x80,并且采样率出现3%偏差的时候,寄存器设置能够正确写入,并能正确读出。