This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1191电极脱落检测

  最近使用ADS1191做一款心电产品,产品需求是只需要通过左右手测试心电信号,所以我们的方案是将右腿驱动电路加了两个10M的电阻分别反馈到两个电极输入端LA,RA上,具体电路图参见附件中的ADS1191的应用方案。

     具体寄存器设置情况:

   0X50,// ID;

   0X01,// CONFIG1;

   0XE0,// CONFIG2;

    0X34,// LOFF;

    0X50,// CH1SET;

    0X80,// CH2SET;

 0X33,// RLD_SENS;

 0X03,// LOFF_SENS;

 0X00,// LOFF_STAT;

 0X02,//MISC1;

 0X02,// MISC2;

      但是在这种情况下并不能检测到电极脱落,而是一直检测到电极是扶好的。请问这种问题如何解决。希望各位大神予以帮助!

PS:1.我们曾尝试将两个10M的反馈电阻换成20M的电阻,这样,在相同的寄存器设置的情况下,是可以检测到电极脱落的,但是这种情况测试出的的心电信号受共膜信号的影响好像比较大,杂波比较多。

PS:2.这个问题能不能通过调整03H寄存器的高三位bits【7:5】来解决?只是对这个寄存器中高三位定义的各个百分比的电极脱落比较阈值的概念以及比较器的结构不是很了解。各种文档中并没有详细的介绍,还请各位高手出手相助。