Other Parts Discussed in Thread: ADS1292, ADS131A02
在做一个设计,需要至少22位的ADC(1.8mV的分辨率),输入的是一个差分信号(±1.5V)和一个temp信号(温度信号已经转换成了电压信号)。有没有单电源供电的双通道的ADC满足我这个设计条件啊?我在选型里面筛选了好久都没有找到合适的,要不就是双电源供电(需要参考电压也算双电源),要不就是输入的模拟电压信号太小等等,是否有用过此类产品推荐。
输出信号类型最好是SPI,I2C,UART之类的最好不过了,可以直接接到MCU。
采集的模拟电压范围是±1.5V,采样速率只要大于2KHz就行,通道数2个,因为是一对差分信号,一个温度信号。我选了很久了。希望是单电源供电,具体电压值没有要求,不过我采集的电压差都有3V了。
我自己选了两款ADC ADS1292和ADS13A02,请问这两款主要的区别有哪些?我数据手册看怎么看懂。另外有跟好的ADC也可以推荐下