Other Parts Discussed in Thread: OPA350
电路参考的是手册里厕所。基准芯片用的REF5025,后面接的OPA350驱动,电容130UF左右,到ADC处正负分别串联49.9欧电阻再到差分基准输入脚。上电后能正常运行一两分钟,然后发现采集数据乱跳,测量基准脚电压后,发现基准引脚处电压0.6到2.5之间乱跳。然后直接量OPA350输出的地方电压很稳定是2.5V。把两个49.9欧电阻直接短接后,再量基准引脚上的电压,只有0.4V左右,上电不到20秒,就发现OPA350芯片很烫。SPI隔离器用的ADUM1401ARZ。前一版电路用的6N137隔离后了有这个问题,发现采集数据乱跳,以为是光耦隔离波形不好,然后这一版换成ADUM1401后同样有问题,才发现是芯片基准引脚处有问题,好像是ADC内部有什么低阻抗东西接在上面一样。请问这是什么原因?
PCB布局上,晶振直接在晶振引脚右边,线长大约15mm左右。晶振是8M
请问有QQ可以联系吗?论坛实时性太差了。我的QQ342186261