Other Parts Discussed in Thread: ADS131E08S
我目前正在用ADS131e08s这个芯片,前4个通道连接外部ADC链路,5-8通道的inp和inn输入都上拉到V+(5通道输入不接外部链路),前4个通道读取外部通道数据,第5个通道读取内部传感器的数值。结果发现,前4个通道的数值都是对的,第5个通道的电压值在2.4V左右波动(使用内部2.4V基准),应用温度转换公式出来的摄氏度值明显不对,而且24位状态码为C1 00 00,第5通道的INP超限,但是我在配置中第5通道是切换到温度测量模式的,而且5通道的gain值也是设置为1,那这样不应该是5通道的INP超限啊,,为什么状态码会显示C1,而且转换结果不对,请问这个是什么原因呢,是否是5通道的inp和inn不应该上拉到V+,应该悬空?应该怎样解决?谢谢!