This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何测试ADC性能

Other Parts Discussed in Thread: ADS1258, ADCPRO

尊敬的TI技术专家,

        您好!我现在用ADS1258做了一块采集卡,请问有比较简单的测试方法来测试我的采集卡的性能和精度吗。

        我现在用普通的信号发生器产生了一个正弦波,1KHz的频率,用采集卡采集了16*1024个数据,请问,我该如何从这些采集到的数据中分析出我的采集卡的精度和信噪比,能否提供一个计算信噪比和精度的matlab的程序。

  • 可以将你的数据输入TI 的ADCPro软件直接进行分析,ADCPro可从下面链接下载:http://www.ti.com/tool/adcpro

  • 你好!

    如果需要得到DUT的S/N、S/(N+THD)等参数,楼主要有一个比DUT,也就是ADS1258 动态范围更高的系统,用以测量信号源的成分,因为信号源输出也有THD+N。楼主直接通过采集卡FFT后计算出来的S/N、S/(N+THD)是包括了信号源的整个链路的S/N、S/(N+THD)。

    楼主可以先通过频谱仪测量信号源输出的S/N、S/(N+THD)参数,然后通过ADS1258采集信号源输出,FFT,减去信号源的THD和N,然后计算ADS1258系统的S/N、S/(N+THD)参数。