可以推荐AD转换芯片:要求输入范围0-10V,12位。想做AD转换模块,输入0-10V或者4-20mA,利用开关将电流信号转换为电压,已看了tida365,请求原理的详细讲解。目前选用AD芯片AD7895,但它的输入电压范围为正负10,有点浪费。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看下ADS8512 这款, 多种输入范围的选择,The converter can be configured for a variety of input ranges including ±10 V, ±5 V, 0 V to 10 V, and 0.5 V~4.5V。