This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274短接AINN和AINP,输出2Hz谐波

Other Parts Discussed in Thread: THS4521, ADS1274, REF5025

各位老师好!

        最近在做一个项目,用到ADS1274,前期用的TI官方推荐电路,ADS1274前端加THS4521芯片,但由于THS4521温漂太大(2uV/℃),弃用了,换了LTC2053(50nV/℃)。上述是小插曲,关键问题见下文:

        最近做了挺多实验,发现AD采出的数据一直有较大噪声,软件滤波前在200uV左右,软件滤波后噪声在20-32uV,采集数据通过Matlab分析后,发现噪声频率集中在2Hz,以及2Hz的多次谐波。并且以下几种实验环境结果均一致(除了部分情况谐波幅值不同,这个正常)

  1.          分别用了不同的电源供电
  2.          短接ADS1274 的AINN和AINP
  3.          短接LTC前端+、-

其中ADS1274和LTC2053采用REF5025输出作为参考源,换了不同电源和电源模块。短接ADS1274 的AINN和AINP依然有同频率谐波。

求教各位老师又没遇到过类似问题,或者给出进一步测试和整改思路。谢谢!

其matlab分析如下图