This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278无DRDY信号输出

Other Parts Discussed in Thread: ADS1278

现象描述如下:
1.ADS1278的供电5V、3.3V、1.8V输入正常
2.ADS1278晶振使用25MHZ,输出正常
3.模式配置:MODE[1:0]:[0,0],选择高速模式
4.模式配置:FORMAT[2:0]:[0,0,1]选择SPI TDM模式 FIX模式
5.同步信号:8KHZ的脉冲,一个周期内,低电平维持时间:10us

问题:只要给同步信号,低脉冲时间符合要求,DRDY信号应该会有下降沿输出(数据准备好),现在DRDY一直维持高电平

ADS1278.pdf