Other Parts Discussed in Thread: ADS803
尊敬的IT工程师,你好!
我现在想设计一个输入范围为1.5V-3.5V的驱动电路。
我从图八里面看到,#IN要接上一个外部的+2.5V,是不是直接接上CM就可以了?是不是其实CM只是为了方便,引出来的参考电压。如果需要其他幅值的参考电压时,就必须要用到REFT和REFB,或者外部参考来实现?
还有,是不是设置了2V峰峰值之后,#IN=+2.5V。当输入为+3.5V时,输出为FFF?当输入为+1.5V时,输出为000?