Other Parts Discussed in Thread: ADS1675
TI的工程师你们好,我现在写ADS1675进行高速采集的程序,看时序图应该会使用PLL进行3倍频,但是这个PLL需要配置吗?一直达不到我想要的结果。谢谢大哥们,帮帮小弟呀
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1675
TI的工程师你们好,我现在写ADS1675进行高速采集的程序,看时序图应该会使用PLL进行3倍频,但是这个PLL需要配置吗?一直达不到我想要的结果。谢谢大哥们,帮帮小弟呀
The high-speed modes (DRATE = 100, 101) are supported in high-speed LVDS interface mode only. The state of the LVDS pin and the SCLK_SEL are ignored. In these two modes, an on-chip PLL is used to multiply the input clock (CLK) by three, to be used for the serial interface. This high-speed clock enables all 23-bit output data to be shifted out at the high data rate. The DRDY pulse in this case is three serial clocks wide. The on-chip PLL can lock to input clocks ranging from 8MHz to 32MHz. To conserve power, the PLL is enabled only in the high-speed modes. After power up as well as after the CLK signal is issued, if the CLK frequency is changed, and when switching from low-speed mode to high-speed mode, the PLL needs at least tLPLLSTL to lock on and generate a proper LVDS serial shift clock. Switching among the high-speed modes does not require the user to wait for the PLL to lock. While the PLL is locking on, DOUT and SCLK are held low. After the PLL has locked on, the SCLK pin outputs a continuous clock that is three times the frequency of CLK.
设置高速模式就可以