Other Parts Discussed in Thread: ADS1675
真心求救一下工程师们,ADS1675高速模式采样程序,感觉自己写的没有问题,现在问题主要是倍频不上去,求工程师们帮忙看一下程序!
----------------------------------------------------------------------------------
-- Company:
-- Engineer:
--
-- Create Date: 08:53:13 06/10/2019
-- Design Name:
-- Module Name: ADC1675_1 - Behavioral
-- Project Name:
-- Target Devices:
-- Tool versions:
-- Description:
--
-- Dependencies:
--
-- Revision:
-- Revision 0.01 - File Created
-- Additional Comments:
--
----------------------------------------------------------------------------------
library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.STD_LOGIC_ARITH.ALL;
use IEEE.STD_LOGIC_UNSIGNED.ALL;
-- Uncomment the following library declaration if using
-- arithmetic functions with Signed or Unsigned values
--use IEEE.NUMERIC_STD.ALL;
-- Uncomment the following library declaration if instantiating
-- any Xilinx primitives in this code.
--library UNISIM;
--use UNISIM.VComponents.all;
entity ADC1675_1 is
Port (
AD_CLK : in STD_LOGIC; --ADC时钟输入
CS : out STD_LOGIC;
START_1 : out STD_LOGIC;
DRATE_0 : out STD_LOGIC;
DRATE_1 : out STD_LOGIC;
DRATE_2 : out STD_LOGIC;
FPATH : out STD_LOGIC;
LL_CONFIG : out STD_LOGIC;
LVDS : out STD_LOGIC;
SCLK_SEL : out STD_LOGIC;
PDWN : out STD_LOGIC;
ADOUT : out STD_LOGIC_VECTOR(23 downto 0);
ADC_DRDY : in STD_LOGIC;
-- DRDY : in STD_LOGIC; -- /DRDY_1
AD_DOUT : in STD_LOGIC;
-- DOUT : in STD_LOGIC; --/DOUT_1
AD_SCLK : in STD_LOGIC
-- SCLK_N : in STD_LOGIC --/SCLK_1
);
end ADC1675_1;
architecture Behavioral of ADC1675_1 is
type states is (init,start,decide_2,data,work);
signal state : states := init;
type states1 is (clk_int,delay,clk_wait,clk_star);
signal state1 : states1 := clk_int;
signal START_11 : std_logic;
signal datreg_value : std_logic_vector (23 downto 0); --24位数据
signal acqdat_count : std_logic_vector(4 downto 0);--采集数据计数
signal counter : std_logic_vector(10 downto 0); --PLL延时计数
signal one : std_logic; signal two : std_logic; signal three : std_logic; signal four : std_logic; signal five : std_logic; signal six : std_logic;
signal seven : std_logic; signal eight : std_logic; signal nine : std_logic; signal ten : std_logic; signal eleven : std_logic; signal twelve : std_logic;
signal thirteen : std_logic; signal fourteen : std_logic; signal fifteen : std_logic; signal sixteen : std_logic; signal seventeen : std_logic; signal eighteen : std_logic;
signal nineteen : std_logic; signal twenty : std_logic; signal twenty_one : std_logic; signal twenty_two : std_logic; signal twenty_three : std_logic; signal twenty_four : std_logic;
begin
process (AD_CLK)
begin
IF (AD_CLK'event and AD_CLK = '1') then --启动配置
case state1 is
when clk_int =>
PDWN <= '1';--上电
CS <= '0';--芯片未选择 单通道
DRATE_0 <= '1'; -- 控
DRATE_1 <= '0'; -- 制
DRATE_2 <= '1'; -- 速度
FPATH <= '0'; --
LL_CONFIG <= '1';
LVDS <= '0';
SCLK_SEL <= '0';
START_11 <= '0';
state1 <= delay;
when delay =>
if(counter = "11111100000") then
counter <= "00000000000";
state1 <= clk_wait;
else
counter <= counter +1;
state1 <= delay;
end if;
when clk_wait =>
if(ADC_DRDY='1') then
START_11 <= '1';
state1 <= clk_star;
else
START_11 <= '0';
state1 <= clk_wait;
end if;
when clk_star =>
START_11 <= '1';
state1 <= clk_star;
end case;
end IF;
end process;
process (AD_SCLK)
begin
IF (AD_SCLK'event and AD_SCLK = '1') then
case state is
when init =>
acqdat_count <= "00000";
datreg_value <= X"000000";
state <= start;
when start =>
if (START_11 = '1') then
START_1 <= '1';
state <= decide_2;
else
START_1 <= '0';
state <= start;
end if;
when decide_2 =>
if(ADC_DRDY = '1') then
twenty_four <= AD_DOUT;
acqdat_count <= "00001";
state <= work;
else
state <=decide_2;
end if;
when work =>
case acqdat_count is
-- when "00000"=>
-- twenty_four <= AD_DOUT; acqdat_count <= "00001"; state <= decide_2; --1
when "00001"=>
twenty_three <= AD_DOUT; acqdat_count <= "00010"; state <= work;
when "00010"=>
twenty_two <= AD_DOUT; acqdat_count <= "00011"; state <= work;
when "00011"=>
twenty_one <= AD_DOUT; acqdat_count <= "00100"; state <= work;
when "00100"=>
twenty <= AD_DOUT; acqdat_count <= "00101"; state <= work;
when "00101"=>
nineteen <= AD_DOUT; acqdat_count <= "00110"; state <= work;
when "00110"=>
eighteen <= AD_DOUT; acqdat_count <= "00111"; state <= work;
when "00111"=>
seventeen <= AD_DOUT; acqdat_count <= "01000"; state <= work;
when "01000"=>
sixteen <= AD_DOUT; acqdat_count <= "01001"; state <= work;
when "01001"=>
fifteen <= AD_DOUT; acqdat_count <= "01010"; state <= work; --10
when "01010"=>
fourteen <= AD_DOUT; acqdat_count <= "01011"; state <= work;
when "01011"=>
thirteen <= AD_DOUT; acqdat_count <= "01100"; state <= work;
when "01100"=>
twelve <= AD_DOUT; acqdat_count <= "01101"; state <= work;
when "01101"=>
eleven <= AD_DOUT; acqdat_count <= "01110"; state <= work;
when "01110"=>
ten <= AD_DOUT; acqdat_count <= "01111"; state <= work; --15
when "01111"=>
nine <= AD_DOUT; acqdat_count <= "10000"; state <= work;
when "10000"=>
eight <= AD_DOUT; acqdat_count <= "10001"; state <= work;
when "10001"=>
seven <= AD_DOUT; acqdat_count <= "10010"; state <= work;
when "10010"=>
six <= AD_DOUT; acqdat_count <= "10011"; state <= work; --19
when "10011"=>
five <= AD_DOUT; acqdat_count <= "10100"; state <= work;
when "10100"=>
four <= AD_DOUT; acqdat_count <= "10101"; state <= work;
when "10101"=>
three <= AD_DOUT; acqdat_count <= "10110"; state <= work;
when "10110"=>
two <= AD_DOUT; acqdat_count <= "10111"; state <= work;
when "10111"=>
one <= AD_DOUT; acqdat_count <= "00000"; state <=data;
when others => null;
end case;
when data =>
ADOUT <= twenty_four&twenty_three&twenty_two&twenty_one&twenty&nineteen&eighteen&seventeen&sixteen&fifteen&fourteen&thirteen&twelve&eleven&ten& nine&eight&seven&six&five&four&three&two&one;
state <= decide_2;
end case;
end IF;
end process;
end Behavioral;