This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS1209扫描工作模式下转换结果的读出



1、数据手册第16页给出的双通道扫描模式的时序图中,READ信号是芯片内部产生的信号还是外部施加的信号?如果是内部产生的,第19管脚的/RD信号需要施加怎样的信号?按照说明,数据是在每个时钟的下降沿自动出现在数据总线上?

2、如果在第一个CONV_CLK 周期进行读操作,读出的数据虽然无效,但是否是允许的?

3、如果在最后一个CONV_CLK时钟周期结束时停止读操作,很明显还有4个转换好的数据没有读出,如果不改变控制寄存器的设置,下一次施加CONV_CLK时,前4个时钟周期是否可以把上次未读出的4个数据依次读出来?

感谢!

  • Hi Yixin Ma,

    1.Read信号由外部施加,具体时序图见数据手册图29,数据会在每个/RD信号的下降沿后出现在数据总线上。

    2.虽然无效,但是允许。

    3.只要没有进行过重置操作,下次施加CLK时的确会将前一次未读出的4个数据读出。