Other Parts Discussed in Thread: DAC81408
在数据手册中,DAC81408的建立时间为12uS
而爬升速率0~5V为1V/uS,如果控制输出从0V跳变至5V,以此时间计算,时间为5uS,小于12uS的建立时间典型值
如上图所示为数据手册中建立时间曲线,±20V输出,如果按照数据手册中4V/uS爬升速率计算,0到20V跳变时间为5uS,从以上两图页可以看出,信号在5uS内达到设定值20V,该时间也小于建立时间典型值12uS。
请问如何理解数据手册中的12uS建立时间这个参数呢