Other Parts Discussed in Thread: ADS1118, ADS1118EVM
完全按照手册《Precision Thermocouple Measurement with the ADS1118》和《Ultra-Small, Low-Power, SPI-Compatible, 16-Bit ADC and Temp Sensor w/ Int Ref》描述制作了电路板并写了程序。
问题现象:
PGA为16倍放大时,信号发生器给固定mV值,用示波器观察SPI的Dout,D15-D9很稳定,D8-D0变化很大;
PGA为8倍放大时,信号发生器给固定mV值,用示波器观察SPI的Dout,D15-D7很稳定,D6-D0变化很大;
PGA为8倍放大时,信号发生器给固定mV值,用示波器观察SPI的Dout,D15-D5很稳定,D4-D0变化很大。
MCU输出信号的波动与上述各个放大倍数下采集值的波动情况能对应的上:用16倍放大时,波动最大,用2倍放大时相对好一些。
因为我没有买ADS1118EVM。我的问题是:用TI的评估板ADS1118EVM做上面同样的测试,结果是不是和我描述的一样,因为我看评估板所用电路和手册上的也是一样的——我是严格按手册上描述加工的实验板。
如果用评估板做的上述测试比我的结果要好,那么,自己制作ADS1118的实验板,除了按照手册上说的进行,还需要注意些什么。