Other Parts Discussed in Thread: ADS8568, TMS320C6657
各位好,
请问ads8568与DSP的并口引脚怎么连接的吗?主要是AD上busy、convst、cs、rd、wr这几个控制引脚和dsp并口引脚的这些信号upp_clk,upp_enable,upp_start,upp_wait应该是怎么连的?或者说部分引脚用普通I/0口就可以了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8568, TMS320C6657
各位好,
请问ads8568与DSP的并口引脚怎么连接的吗?主要是AD上busy、convst、cs、rd、wr这几个控制引脚和dsp并口引脚的这些信号upp_clk,upp_enable,upp_start,upp_wait应该是怎么连的?或者说部分引脚用普通I/0口就可以了?
你好,我调试的ADS8568使用的是SPI与mcu进行通信,仅通过SDO_A作为数据输出:
1、测量电压功能的功能很正常,16bit的数据能够从SPI总线收取到,并且结果正确。
2、读取和设置内部的Configuration (CONFIG) Register存在问题,按照datasheet上所述,更新或读取寄存器需将对应的bit设置为1,但按此配置读取寄存器内容为随机数值,明显与默认值0x000003FF不符。
在代码中读取的时序为:
spi.write([0xC0, 0x00, 0x3F, 0xFF])
data = spi.read(4)
请帮忙看下读取的时序是否有问题,或者配置是否有问题