Other Parts Discussed in Thread: ADS1274
第一次用ADS1274做项目,这几天在调试时遇到一个困扰我的问题,1.AINN管脚输入:取2.5V基准电压采用OP1177运放组成跟随电路,在AINN上得到2.500V电压 2.AINP输入端为我的信号放大电路信号接入。3.在AINN和AINP之间接入一个2.2nF的电容。出现的问题是这样:无论我的AINP输入端输入多大的值,在AINP脚都测不对输入信号,例如我输入2V,采集数据不是2V,用电压表测量AINP电压值为2.41V,我自己猜测可能是S1、S2短路,请问这是什么原因造成的?