Other Parts Discussed in Thread: DAC7716
你好,我最近在使用贵公司的DAC7716芯片,使用过程中出现了一些问题:
参考电压:5V,
AVSS=-15V;
AVDD=+15V;
UNI/BIP接地;
RFB1-X与VOUTX相连,RFB2-X悬空;
配置COMMAND寄存器的值为0x033C;
当设置DAC-0的input 寄存器的值为:0x7FF0时输出是+10V;
设置DAC-0的input寄存器的值为:0x8000时输出是-5V左右。
问题:
我所有的模式都是按照双极性-10v~+10V配置的,为何我设置DAC-0的input寄存器的值为:0x8000时输出是-5V左右。这里得到的结果不应该是-10V吗?
在线等,请尽快回复,谢谢!