Other Parts Discussed in Thread: DAC3161, DAC3174
DAC3161在应用中若要使用IO TEST该怎么用?我现在能输出正常波形,但温度变化过大后,可能会有FPGA和DAC数据接口时序不匹配问题。调整寄存器延时后又能恢复正常。所以想用DAC芯片内部的IO TEST功能实现接口时序先验证再工作。但无论怎么配置都无法正常使用该功能。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您的耐心等待,附件PPT它详细介绍了IO TEST功能设置DAC的步骤。另外链接了一个旧的E2E帖子,在那里我们讨论了如何让IO TEST正常工作。
PPT中的步骤已经测试过了,并且能够使用DAC3174的IO TEST 功能。这些说明也适用于DAC3161,因为它与DAC3174属于同一系设备