Other Parts Discussed in Thread: DAC8771, DAC8771EVM
1)在使用DAC8771中我开启了内部buck---boost,数据手册8.3.3.2中说明,When used in voltage output mode, the Buck-Boost converter generates a constant ±15.0 V for the positive andnegative power supplies.,当在电压输出模式下使用时,Buck-Boost转换器为正负电源产生恒定的±15.0V。
2)而我测量正负电源的电压正电压VPOS 11V左右,负电源VNEG 0.48V
3)DAC8771数据手册7.3节说了在电压输出模式下,VPOS范围【-0.3 +33V】,VNEG范围【-18 -5V】。
4)当我关闭buck----boost电源的时候,VPOS居然还是有3V的电,VNEG有0.3V的电。(在我理解的是,我关闭了buck---boost电源,内部应该不会有电输出)
5)数据手册说12------36V给芯片供电都可以,但是我发现当我把电源调到15V或者以上,芯片就会非常发烫。
6)以上迹象是否说明该芯片电路工作不正常。电路原理图在附件0601.气动控制驱动控制V2.0.pdf