Other Parts Discussed in Thread: ADS1274, THS4521
您好!
我在调试ADS1274时发现一些问题,
1、采直流信号的时候偶尔会采到一些偏小很大的值,比如正常值是40000左右,偶尔会采到几千甚至几百的值,
2、当输一个几Hz到几百Hz的方波脉冲信号时,脉冲的占空比1%-99%不等,在脉冲信号的上升沿和下降沿附近会采到几个接近0或者超过8300000的值(像是满量程了),正常值应该是1700000左右,示波器抓取THS4521输出的差分信号是比较平滑的,并没有什么高的毛刺,用逻辑分析仪抓取Dout输出信号可以确认不是SPI读数的问题,每一个通道都这样,所以请帮忙分析一下这是什么情况,谢谢!
ADS1274使用mode[1:0]=01高分辨率模式,format[2:0]=001 SPI/TDM/Fixed,输入时钟27MHz,SPI采样时钟13.5Mhz,数据是先采样缓存在RAM里面再一次性打出来的,所以不存在因为打log而导致断点的问题
图一:ADS1274采样原始数据描出来的波形,只在中间采对了2个点约1700000的值
图二:脉冲信号经过THS4521后输出的差分信号波形