Part Number: ADS1120
测试温度信号时,NTC传感器通过用电压源,串联电阻分压来测量电阻。PT100或者PT1000传感器通常用电流源做激励,来测量温度。
为什么NTC传感器通常用电压源做为激励而PT1000这类传感器通常用电流源做为激励呢?
Can I ask why NTC sersor often use volatge source while PT100 use current source ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1120
测试温度信号时,NTC传感器通过用电压源,串联电阻分压来测量电阻。PT100或者PT1000传感器通常用电流源做激励,来测量温度。
为什么NTC传感器通常用电压源做为激励而PT1000这类传感器通常用电流源做为激励呢?
Can I ask why NTC sersor often use volatge source while PT100 use current source ?
您好,
我找到了下面链接NTC温度测量电路和ADS1120手册中的Pt100测量电路,对比后我认为这个主要在于传感器的输出电阻范围,具体传感器考虑具体的方法。
Pt100的电阻输出范围是0~400Ω(温度范围-200℃~ 1000℃),而下面链接NTC给出的电阻范围是819.7Ω~ 2.252 kΩ温度范围是50 ℃~ 25℃,注意温差仅25℃
对比2个测量电路,Pt100电流激励的测量电路相对比较复杂(ADC需要的输入接口比较多),这应该是为了提高测量的精度,因为Pt100温度变化这么大范围,输出电阻仅变化400Ω,如果采用类似这里NTC的测量电路,那么电路中R1的值就需要选择的比较 小,那么在电阻上消耗的发热功率就比较大,一方便影响系统效率,一方面发热影响测量精度;
而NTC采用Pt100测量电路,可能需要考虑输入信号范围和输入的共模电压等是否满足要求,一般来说,可以使用简单的电路满足测量要求,就没必要使用相对复杂的电路了。