经测试发现ads8866采集电压有20mV波动,电压采用是德科技U3606B输出的0.2V;然后ads8866 1s读取一次电压,一共采集了927组数据,用数据中最大值减去最小值大概是22mV左右;电路图和数据如附件ads8866测试数据.xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
经测试发现ads8866采集电压有20mV波动,电压采用是德科技U3606B输出的0.2V;然后ads8866 1s读取一次电压,一共采集了927组数据,用数据中最大值减去最小值大概是22mV左右;电路图和数据如附件ads8866测试数据.xlsx
您好,
AD转换输出存在误差除了ADC本身的精度有关外,也与基准电压、供电电压是否稳定、纹波大小有关系,也与输入信号是否干净稳定有直接关系,所以建议您用示波器测量输入信号、基准电压和供电电压存在的纹波是否比较大、是否稳定
另外,请注意,输入滤波电路较高的RFLT值有助于提高放大器的稳定性,但由于与ADC的非线性输入阻抗相互作用,会增加失真。失真随着源阻抗、输入信号频率和输入信号振幅的增加而增加。参考datasheet 10.1.2.2 Charge-Kickback Filter部分(A higher value of RFLT helps with amplifier stability, but adds distortion as a result of interactions with the nonlinear input impedance of the ADC. Distortion increases with source impedance, input signal frequency, and input signal amplitude.)
我的基准和电源都是Ldo输出的,输入信号也用Ldo模拟的直流电,输入滤波器的rc按照手册所写现在换成了10r和1nf;目前采集做到Vpp是3mV的波动,这正常吗?你们demo板能做到多少?
抱歉,我手头上没有ADS8866 的demo板无法进行这样的测试,但是我认为您这个实现的已经很好了,看下面ADS8866电气性能,仅失调误差就4mV max了
也就是说您的输出波动范围是±1.5mV,如果失调误差是0V的话,那么这±1.5mV的误差就是我上述提到的因素造成的,那么您可以附上供电电源、基准电压和输入电压的纹波测试图吗?同时请将纹波幅值和频率显示出来