Part Number: ADS1299
请问我用两片ADS1299进行级联连接形成16通道数据采集,但是我配置好第二片寄存器后,发出START指令后不能正确读到数据,读到的数据都是0,而且DRDY引脚只拉低一次。CS选择第一片的时候能够读到数据
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
启动转换后,您片选CS1(device1的CS),device1的DRDY就会拉低说明已转换完成,那么就可以发出时钟,去读取device1的转换结果,如果device1的转换结果是正确的,那么device1是正常工作的,然后仅片选CS2(device2的CS),[ 因为device1和device2是同时启动转换,那么2片的DRDY是相同的信号,因此仅连接device1的DRDY至主控端,节省一个主控端的GPIO;因为CS信号对DRDY信号没有影响,CS不拉低,对应的device的DOUT就是高阻态,因此通过拉低相应的CS去读取相应的device的转换输出],然后发出时钟,去读取device2的转换结果,如果device2的转换结果是正确的,那么device2是正常工作的