This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1232: 对差阻式传感器进行测量数据跳动大,约有11位在跳动

Part Number: ADS1232

使用的是12V输入,通过7805转换为5V,再通过LM117-3.3转换为2路3.3V,分别给模拟电路和数字电路供电,通过2.5V基准产生2.5电压,再通过运放设计成恒流电路测量差阻式传感器的两个电阻,想要通过模拟开关切换来测量不同差阻式传感器的电阻,目前发现电路采集到的电压跳动很大,只有前面13个数字是稳定的,24位ADC做到16到18位稳定不难吧,请问这是我哪里设计需要改进的吗?另外就是2路模拟开关,一路接传感器,另一路未接传感器时测未接传感器这组的数据时也能测到电压,电压大小与接传感器那组测到的数据相近。

  • 您好,

    ADS1232采集信号时,存在约有11位在跳动是一直存在这个跳动吗?还是仅在切换输入前后那端时间里存在跳动?或者说不切换输入信号时,也一直存在这个11位跳动吗?

    ADS1232的输入信号RED、BLACK、GREEN是经过模拟开关 ADG715 输入的,那么模拟开关 ADG715很可能会对源端输入信号造成影响,您是否用示波器测量ADS1232输入管脚端的信号,看是否与期望值一致?是否存在波动?

    另外就是2路模拟开关,一路接传感器,另一路未接传感器时测未接传感器这组的数据时也能测到电压,电压大小与接传感器那组测到的数据相近。

    这不排除是模拟开关串扰造成的影响,建议断开ADS1232的传感器的输入信号,让ADS1232输入端直接采集已知的直流信号,看采集信号是怎样的?以排除前级电路对采集信号的影响

  • 断开模拟开关直接传感器连到ADS1232信号输入口是有7位在跳动,连上模拟开关就不行了,所以我在想是我模拟开关在这里用的不对吗?

  • 一般来说,模拟开关都有开通和断开时间,或者说开通和断开时,对输入信号相当于突变,它需要有个稳定时间,因为ADG715是ADI的产品,具体您可以咨询ADI的技术支持

  • 在3.3v的供电电压下,你的恒流源无法驱动你的传感器桥路。换句话说,你的恒流源做不到2.5mA恒流,所以会造成ADC跳动。你可以算一算你的电压余量: 3,3v电源- 恒流源取样电阻压降2.5V - 恒流调整三极管CE压降,可能只有0.xV留给传感器。