This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1230: 输出数据会不定时出现一个异常数据

Part Number: ADS1230

我们现在在使用ADS1230芯片。在使用过程中一直没什么问题。最新一批产品出现了,输出数据会不定时出现一个异常数据的问题。换了原来的ADS1230芯片后正常。

我们抓波形发现,这些异常数据出现后,会暂停一段时间的数据发送。在示波器上显示会有一个断档。下图中的波形出现了2个空挡。

这个数据之后其它数据就正常了,我们采用80Hz的频率采样。

请问这是什么问题?

  • 波形说明:

    1箭头 2箭头 —— 两次异常数据出现后的ADS123暂停输出数据(Data Ready脚一直为高)。

    2.1箭头 2.2箭头—— 是2箭头数据的Zoon

    2.1箭头 —— 异常数据

    2.2箭头 —— 正常数据

  • 您好,

    黄色通道是DRDY/DOUT信号是吗?应该在DRDY/DOUT的下降沿表示data ready,但是在2.2箭头处data ready下降沿没有发出SCLKs(绿色通道是SCLK信号吗?)信号去读取数据?

    2.1箭头是DRDY/DOUT是高电平,说明转换数据还没ready