Part Number: AFE44S30
Other Parts Discussed in Thread: AFE4404EVM, , AFE49I30, AFE4950, , AFE4404
您好
我在贵公司购买过AFE4404EVM,根据数据表,它的LED电流为0-50mA(最高可扩展到100mA),而实际上我们使用它测试血氧浓度时电流是低于10mA的,现在我计划购买AFE44S30EVM,根据数据表,这款产品的LED电流范围是25-250mA,另外的型号比如AFE4950、AFE49i30的LED电流范围均为25-250mA,为何这一电流范围相较于AFE4404有很大不同?若我要使用AFE44S30,在小于25mA的电流下LED是否能正常工作?我们也对如此大的电流感到疑惑,如此大的电流可以应用于什么场景下呢?
期待您的回复,谢谢!