Other Parts Discussed in Thread: ADS1232
老师你好,现在使用ADS1232进行电压信号采集,目前我是采用三线制DOUT,SCLK,PDWN通过单片机IO口进行控制,手册上有6种时序图,但只有最后时序图体现有PDWN,请问前面的几种模式PDWN应该怎样处理?
我目前的理解是手册fig41是初始化,其他fig34-38的时序是正常数据转化的时序,现在主函数中每次进行初始化,PDWN拉低再拉高等待400ms,然后转化可以正常。如果改为上电只一次初始化,然后查询方式连续读数据,结果出现多个不同的数据跳变显示出来,因为ads1232没有数据寄存器,那其他的数据是从哪里得来的,是我一次读出了多次转化的结果吗,请老师指教