This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S06: 推荐

Part Number: ADS124S06
Other Parts Discussed in Thread: ADS1120,

您好,

    想使用三线制PT100实现测温精度在0.1℃以上,请问有推荐使用此需求的ADC吗?

    看到论坛上提到的ADS1120等芯片均是以前好久的产品,需要推荐性能稳定,测温精度高的ADC。

 谢谢!

  • 您好,

    在ADS124S06 数据表如下截图部分,是不是说明10.2 Typical Application的典型应用可以实现精度为±0.024°C的测量?

  • 您好,

    不太清楚。

  • ADS124S06 比例测量其实是测量的温度传感器的电阻,电阻误差如数据表图115所示。它是测量的 20 Ω to 400 Ω范围的电阻,电阻误差需要转换为温度误差,计算公式是数据表公式27。数据表给出的计算例子是在 0°C 时传感器灵敏度值计算的。

    您可以根据您需要测量的温度范围,换算出所需要测量的电阻值范围,然后根据您使用传感器的灵敏度计算温度误差,以验证是否满足您的应用温度精度。