Other Parts Discussed in Thread: DAC1280, DAC1282, ADS1281, ADS1282
请问DAC和PWM控制器相比哪个能实现的精度更高?
具体设计为实现0.12v-0.3v的可调电压,调节精度大概在0.01mv。
请问哪种DAC或PWM可以实现这个要求?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的2款24bits DAC是 DAC1282和 DAC1280,DAC1280是输出电流模式的。
DAC1282是输出电压模式的,有以下4中输出模式:sine、DC、Digital data和脉冲。您需要输出的PWM,低电压是0.12V,高电压是0.3V吗?
如果要求调节精度大概在0.01mV,那么所选DAC的分辨率至少低于0.01mV。
另外,DAC1282是与ADS1281、ADS1282一起搭配应用于地震数据采集系统的,其噪声性能可能差一些。