This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220: IDAC1和IDAC2恒流源不一致

Part Number: ADS1220

尊敬的TI工程师!

在使用ADS1220的时候发现一个问题,通过AIN1和AIN2通道出来的电流与AIN3出来的“电流不一致”?

设置参数如下:寄存器0~寄存器3分别为,0x46 0x04 0x55 0x50

AIN3端负载电阻为1K,AIN1和AIN2端为RTD,大小估计为1.1K,实际测试,RTD两端电压正常,为0.55V,可是AIN3端的电压只有0.3V,请问是什么原因呢?

期待回复!!!