问题1:DAC8830输出电压一直保持不变;
问题2:DAC8830上电,输出不复位到0,输出电压值是上次断电前输入的数据;
SPI引脚时序图SDI与SCLK,SCLK与CS,由于只有两通道示波器,所以分成了两次抓拍了这三个引脚了时序;
上图为DAC8830上电就输出一个电压值,没有上电复位到0,波形绿色为电源,黄色为输出电压;
上图为电路设计图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、电路图中AGND与AGND1两个地是通过一个0欧姆电阻单点连接的;
2、DAC8830输出电压一直保持不变,电压值是上一次断电前的输入数据;比如现在给DAC8830输入0xFFFF,但是输出不刷新,现在断电然后再上电,此时上电后输出的电压2.5V,现在给DAC8830发数据0x8000,输出不刷新,现在重新上电,输出电压刷新为1.25v;
3、DAC8830基准电压VREF实际测量为2.5v,是通过基准电压芯片提供;
4、主控端接口用示波器测量,上电后没有数据输入。当单片机程序需要发送数据时才会有数据输入;