如题,请教一下ADS8320如何与STM32f103的SPI连接,因为STM32的SPI只支持8位和16为的传输格式。如果您有驱动,那定是极好的!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
或许你可以到STM32这个系列的控制芯片的论坛上问一下。(没有在TI网站上找到)
ADS8320是16位的ADC, 可以与STM32 SPI 16位的传输格式进行通讯。(一般如果超过16位, 如24位,也可以用3个8位,凑成一个24位,进行数据交流)
看下STM32的SPI引脚是否能兼容5V电平,不能的话就加个电平转换芯片。