Part Number: AFE4404
您好,关于AFE4404的TIA部分,贵公司有无相同功能的独立芯片可以放大PD输出的电流信号,我似乎对于AFE4404中TIA部分的原理不是很理解,以至于使用普通的放大器并不能得到很好的脉搏波电压信号,期待您的解答!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE4404
您好,关于AFE4404的TIA部分,贵公司有无相同功能的独立芯片可以放大PD输出的电流信号,我似乎对于AFE4404中TIA部分的原理不是很理解,以至于使用普通的放大器并不能得到很好的脉搏波电压信号,期待您的解答!
您好,
下面文档是PD信号放大电路的参考设计,有原理 和详细设计过程,也有放大器的选择方法,您可以看下,有具体问题您可以回复帖子反馈;
INP、INM管脚的差分输入电路,datasheet已给出,如下截图,即将单端输入电路对称组合成差分输入;
下面链接是AFE4404的FAQ,其中给出了推荐的LED和PD管

感谢答复!另外的问题
1.我将光学模块替换成自己设计的LED-PD模块与AFE4404 EVM连接测试,关闭LED1、LED3,当软件设置LED2输入电流为11.2mA时,实际测得LED电流仅为1.12mA左右,更换其他电流值也是同样的情况,也就是实际输入电流值是设定值的1/10,请问是什么原理?
2.实验分别测得PD输出电流为0.65μA、最终输出电压最大值为0.65V左右,则根据反馈电阻计算公式RF=Vout/Iin=1000KΩ,与理论值2×50KΩ=100KΩ相去甚远,更改其他电流值结果相同。请问问题出在哪里?是我的计算方式不对还是测试结果有误呢?
1、这个问题应该与LED-PD模块有关,这里的LED压降是多少?驱动电压是什么?
2、上述提到的参数您是怎样获得的?
“更改其他电流值结果相同”是什么意思?增益还是1000kΩ吗?