Other Parts Discussed in Thread: ADCPRO, ADS1258
DIFF0在检测500uV及以下电压时产生严重失真。AD1258_TestData.xlsx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DIFF0在检测500uV及以下电压时产生严重失真。AD1258_TestData.xlsx
您好,
您可以详细说明您描述的测量数据异常或严重失真吗?具体表现形式是什么?
ADS1258EVM-PDK的差分通道0在检测10-1uV的电压信号时与其他差分通道无明显区别,检查数据相对准确,但是在检测小于等于500uV的电压信号时会与信号源数据产生比较大的误差,而同等参数下的差分通道1-7则相对表现稳定。通过ADCPro具体测试数据我已经提交在附件表格AD1258_TestData.xlsx中。
DIFF0接入的是 CD端,AB端为信号发生器输入,并且B点还接入到AGND。R1=R4=100KΩ,R2=R3=104KΩ,R5=400Ω,UCD=UAB/500。
当UAB=500mV时,DIFF1-7都能正确的检查到1mV±1.5%的电压,DIFF0检测已经在0.93mV附近波动。当UAB继续变小时,DIFF0检测的误差越大。
ADS1258只有一路ADC模块,它的8对差分输入是通过MUX进行切换输入的,因此,DIFF0检测的误差大不是ADC的问题,只能考虑是模拟输入差分对走线问题或外接电路的问题;
或者您用DIFF0测试已知稳定DC电压,看采集电压是否准确?