请教各位工程师:
我画了一块主控板,数字地和模拟地用磁珠相连,板上有2片ADS8568,设置在并行模式,即8脚的PAR/SER接低。我有如下问题:
1)如果将ADS8568接到数字地,那地平面分隔比较困难,根据芯片资料(见附件)的第41页的figure 44,8引脚下面是模拟地,那我是否可以通过布线将8脚接到数字地?这样布线可能会比较长。
2)是否可以将8脚接到模拟地?这样是否会导致芯片不正常工作?
这块芯片要4路电源,最郁闷的是14脚和15脚(模拟电源引脚)居然夹在数字引脚中间。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教各位工程师:
我画了一块主控板,数字地和模拟地用磁珠相连,板上有2片ADS8568,设置在并行模式,即8脚的PAR/SER接低。我有如下问题:
1)如果将ADS8568接到数字地,那地平面分隔比较困难,根据芯片资料(见附件)的第41页的figure 44,8引脚下面是模拟地,那我是否可以通过布线将8脚接到数字地?这样布线可能会比较长。
2)是否可以将8脚接到模拟地?这样是否会导致芯片不正常工作?
这块芯片要4路电源,最郁闷的是14脚和15脚(模拟电源引脚)居然夹在数字引脚中间。。。
Hi
你画的是几层板?
对于ADC板块数字信号模拟信号都是要求端点接各自的GND plane, 也就是说PAR/SER是需要端点接数字GND plane的.
你可以参考EVM扳的电路: http://www.ti.com.cn/cn/lit/ug/sbau193a/sbau193a.pdf 第十七页Figure 9, layout上并没有选择接模拟GND.
Hi
可以参考如上layout:
第十四脚的AVDD是走的内层线,第十五脚直接接的芯片PowerPad(芯片的PowerPad是接模拟GND Plane的)
(layout上在datasheet第四十一页也有参考的,你也可以参考)