Other Parts Discussed in Thread: ADS1232
使用ADS1232搭建一个直流采样电路,上电后显示采样值溢出,但是用手,或金属(如示波器表棒)接触电路的信号地时,又显示采样正常了.请问这可能是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1232
使用ADS1232搭建一个直流采样电路,上电后显示采样值溢出,但是用手,或金属(如示波器表棒)接触电路的信号地时,又显示采样正常了.请问这可能是什么原因?
已将芯片重新焊接,情况依旧。。。
另,您说的接地是指接信号地,还是外部机壳地?
您好,我还有个ADS1232的问题.资料上说该芯片在低速采样模式下对50Hz的干扰抑制大于60dB,但是没说高速采样模式下的抑制比,是很小呢,比如20dB,30dB还是根本没有呢?
有精确点的值吗?由于设计要求达到80dB,但现在前级滤波只能提供到60dB,如果达不到要求的话只能考虑换芯片了。
您好!ADS1232资料上在低速采样模式10SPS下对50Hz的干扰抑制会到100dB(内部时钟)。
高速采样模式下的抑制比由您的采样速度和时钟的误差决定,具体您的数据率有多少呢?
如果采用80SPS采样模式的话,对50Hz的抑制能力就比较差了,会远远不如10Hz的采样模式,大约只有24dB左右(计算得出的结果,时钟误差3%)。具体的抑制比需要实测得到。
前端如果陷波器的抑制大于60dB应该能够完成80dB的要求
你好,能否把你的电路图和程序发我一份,我也在做这个,但有好多问题,希望能参照你的看看,非常感谢,我的邮箱502117108@qq.com