在做一个profibus-DP 从站,根据VPC3上的参考电路设计的,485芯片使用的是DS75176,本来完全可以满足DP最高12M波特率的要求,可是后来查资料发现只有一个最大22ns的传输延迟这个参数,又看到有网站上说 DS75176只能传输10M的数据,有没有大神做过??望解惑,不甚感激!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
22ns是指数据延时tPLH和tPHL?这个只是一个从输入到输出的延时而已,并不会影响信号的上升时间和下降时间,对你的系统有很致命的影响?我觉得你可能应该关注一下tr和tf这两个参数,这个才是上升时间和下降时间。这两个时间和负载电容有关,手册上写的是RL=60欧姆,CL=100pF时,tr=tf=18ns。对于12M的信号,周期是83ns,如果负载确实能达到100pF这个量级,18ns的tr和tf确实比较大了。
具体的选型,可以到ti官网查询