This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC124S021时序问题

从datasheet后面的使用知道DIN在SCLK上升沿输入,DOUT在SCLK下降沿输出,而时序图好像显示的是DIN在时钟下降沿输入,DOUT则看不出来,现在只转换IN2,但转换结果都是0,程序如下,请大侠指教,谢谢~

void adc_AI1_AI2_FS5V2(void)

{

  unsigned int i, Channel;
  unsigned int data_ad;
 
     Channel= 8;       //第2通道
     data_ad = 0;  

     GpioDataRegs.GPADAT.bit.GPIO13 = 1;   //时钟上升沿准备输入  1

     for (i = 0; i < 16; i++)
     {
               if (i < 8)    //0-7八个时钟上升沿输入b7-b0  控制寄存器的8位   
        {
             if((Channel&0x0080)==0)
             {
              GpioDataRegs.GPADAT.bit.GPIO14=0;
             }
    else
             {
              GpioDataRegs.GPADAT.bit.GPIO14=1;
             }
         
           Channel <<= 1;   //SDI输入数据移位,从b7开始传,最后传b0
        }

        GpioDataRegs.GPADAT.bit.GPIO13 = 0;    //时钟下降沿输出数据   0
  TimeDelayProgram(4);
    

       if (i >=4)   //第5个时钟周期下降沿输出DB11-DB0为12为AD输出的数字量
       {
        
           if(GpioDataRegs.GPADAT.bit.GPIO15==1)   //输出数据为1
   {
       data_ad = (data_ad<<1)+1;
   }
            else        //输出数据为0
   {
             data_ad = (data_ad<<1);
   }
   RESULT_FS5V2 = data_ad;   
       }

        GpioDataRegs.GPADAT.bit.GPIO13 = 1;   //数据输出完又变为时钟上升沿输入控制寄存器的位
  TimeDelayProgram(4);
      
     } 
    
}