This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8584S: 输入信号范围与resolution问题

Part Number: ADS8584S

你好,ADS8584S使用单电源+5V供电,手册中:Full-scale input span (AIN_nP to AIN_nGND),-5~+5 V; 

当我在AIN_nP脚输入0~+5 V范围的信号时,对应采样分辨率还是16 bits 吗?还是等效只有15bits resolution 了?

可以设置在AIN_nP脚输入0~+5 V范围的信号时,resolution 16bits吗 ?

感谢