Other Parts Discussed in Thread: TLV5636, TLV5616
在使用TLV5636时,选择的内部2.048V参考电压,在转换时总是存在5mV左右的误差,在设置输出0时,也不能正常输出0,输出的是8mV,上电后不加控制线时,在DA输出端同样有电压,为7mV,想请教在线工程师,是什么原因导致的这些现象?会是程序问题吗?我使用SPI驱动的。
-----------------------------
repo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
他的意思是在一段代码内输出总是0吧?我的问题是不能正常输出0?其他输出总存在误差,TLV5616就不存在此问题,具体应该怎么解决?盼解答。
-----------------------
repo
TLV5636手册第4页,EZS最大+/-20mV,就是预期输出0V时,实际输出会有最大+/-20mV的偏差。
TLV5616手册第4页,EZS最大+/-10mV,比TLV5636小,所以实测结果比5636好。