ADS1158 MUXOUT、MUXOUTP、ADCINP和ADCINN这四个管脚什么作用呢,如果我用单端5V供电,2.5V基准源,是否要按照datasheet里那种用运放的接法吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为ADS1158是通过mux(复用器)来实现16通道的,MUXOUTP和MUXOUTN是输入信号经过MUX后的输出,没有任何调理;ADCINP和ADCINN是ADC信号输入管脚,这样做的目的:
1.当需要外部做信号调理时,可以在MUXOUTP/N和ADCINP/N之间加入调理电路;
2. 当不需要外部调理时,可以直接在ADS1158芯片内部实现信号的连接;
这样对应用来说可以非常灵活。
所以要不要接运放,看你对系统性能精度的要求。高的话,最好就接。
你好,不知道您能否看到我的问题?
想请问下,ADS1158如果用差分输入方式,电路应该怎么应用?