Part Number: ADS131E08EVM-PDK
Other Parts Discussed in Thread: ADS131E08, TMS320C6748
我在使用ADS131E08的子板采集数据时,出现了如下问题:
1、正弦波信号的频率是20Hz,但是从我采集的数据来看,信号的频率变成了40Hz;
2、貌似采集不到负半轴的数据,是因为我用5V,3.3V的单极性电源供电的原因吗?
3、从图上看,第一个波形的幅值突然增加了一倍。
希望能够得到Ti的工程师的帮助,非常感谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS131E08EVM-PDK
Other Parts Discussed in Thread: ADS131E08, TMS320C6748
我在使用ADS131E08的子板采集数据时,出现了如下问题:
1、正弦波信号的频率是20Hz,但是从我采集的数据来看,信号的频率变成了40Hz;
2、貌似采集不到负半轴的数据,是因为我用5V,3.3V的单极性电源供电的原因吗?
3、从图上看,第一个波形的幅值突然增加了一倍。
希望能够得到Ti的工程师的帮助,非常感谢!

信号发生器产生的模拟信号频率是20Hz,可以每个周期是含有2bit的,即1hz=2bps。
所以采集到的是按照bps来计算的,图中两个X的位置,其实是一个周期内的2个bit,所以频率20Hz=40bps。
您看下面,两个红色框的位置是一个周期2个bit,所以您读取的40hz实质是换算成速率bps,也就是说1hz=2bps。
我理解的就是您这里读取的40hz实质是40bps。

抱歉,我应该说错了。 您这个还是个+-1V的正弦波。
信号发生器的输出用BNC转杜邦线接到CH7,这个波形是在ch7的输入端测试的是吗?
信号发生器的波形看下。
抱歉回复晚了,我以为是信号发生器输出的波形经过杜邦线之后接到CH7,直接在CH7测试的波形频率翻倍。
是“通过TMS320C6748与ADS131E08EVM通信获取数据,最后导出至电脑中的显示”。这里我没太明白,是DSP和ADC通信,输出的应该是数字信号才对吧?