Other Parts Discussed in Thread: ADS801, ADS805
目前调试ads805e,模拟输入范围设置为0~5V,数据转换都正常,但是经过ads805e转换后的数字量,始终比输入信号小将近20%,这是怎么回事啊?之前用ads801都没有遇到这种问题?着急啊,问题都找了几天了,还没找到原因!!!请高手们指点迷津...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有没有测过R113左边,即IN的管脚电压, 看看是不是和你的CHI_ADin电压一样?
另外测下REFT, REFB和Vref管脚的电压看是不是正常。
先去掉C136,看是不是电容引起的。
如果结果还是一样,测试下+5VA波动有多大,以及AD_CLK的波形发上来。另外测试几组电压值和DAC输出值发上来看看。
去掉C136后,还是一样的,+5VA波动很小,很稳定。
下图:为示波器捕获的ad_clk的时钟,此时钟是由FPGA分频产生的(时钟频率可调,占空比50%),提供给ad的时钟引脚。
下图为输入信号波形(20KHz正弦波,安捷伦万用表测试其有效值=707mV,对应的峰峰值=707*2.828=2000mV)
下面为实测的几组数据:
测试次数 输入峰峰值(mv) 输出峰峰值(mv) 误差(%)
1 2000 1595 -20.25
2 2000 1618 -19.10
3 2000 1601 -19.95
从测试结果:可以看出输出的峰峰值均衰减了近20%,原先定型的产品用ADS801E,幅值误差很准的,但是ADS801E停产,后来就换成ADS805E,就出现此现象。麻烦帮忙分析分析,谢谢啦。
时钟似乎有问题。ADS805是个5V的ADC,CMOS的时钟看上去应该给0~5V的电平,但是现在测量到的时钟幅度只有3V左右。如果可行,看看给一个5V的时钟是否有改善。
你用稳压电源给几个直流信号进去,看看在直流情形下能否采对。另,会不会是信号源的问题?比如输出阻抗之类?做完直流测试,也可以换一台信号源试试。