Other Parts Discussed in Thread: ADS1258, OPA350
尊敬的TI工程师你好,我把我在设计ADS1258采集电路过程中的问题整理成一个WORD文档,放在了附件中,希望您能抽点时间帮我解答下,谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1258, OPA350
尊敬的TI工程师你好,我把我在设计ADS1258采集电路过程中的问题整理成一个WORD文档,放在了附件中,希望您能抽点时间帮我解答下,谢谢了
Hi
你的电路(文档中第二个图)将buffer 运放OPA350 短掉了,此时REFN依旧是-2.5V,REFP电压略低于2.5V, 原因是10k的电阻上有所压降。
建议您采用参考电路(文档中第一个图),这个运用了buffer 运放OPA350 ,REFN是-2.5V,REFP为2.5V,10k电阻因为运放虚断压降可以忽略。
按照您的电路,实际上可以仅仅用REF3125 和0.1uF+10uF的参考bypass电容即可。
不好意思,第二个图是我连接失误,OPA350的连接和参考图一致,反馈接负端。
仅仅用REF3125 和0.1uF+10uF的参考bypass电容,输出的只是+2.5V吧,负电压怎么产生呢?我要采集的是双端信号
麻烦您也解答下文档后面的问题吧,谢谢
另外,我想再咨询下,关于产生±2.5V、±5V参考电压的问题,有没有推荐的典型芯片和典型电路。
谢谢
产生正的参考电压,可以考虑REF5025,REF5050。5系列的电压基准芯片,比3系列的噪声和温飘都要小一些。
Hi
如果您需要+/-2.5V,或者可以用REF5050, 因为REF5050 GND接AVSS-2.5V, 所以其输出将是2.5V, 按照REF3125的电路产生的是+/-2.5V的参考电压,实际是5V参考电压。 但是要注意此时的运放,因为输入的不再是0V,而是2.5V,供电就需要改变了。